View the revision history and current versions
for EZtouch software and panel firmware (
PDF document).
Visit the firmware download page to grab the latest EZTouch firmware update
IMPORTANT! Please read the information below before installing an upgrade. This download will upgrade your existing EZTouch programming software to version 3.1-A.
Do not delete any existing EZTouch files!! This is a maintenance release, not a full install. You must have a previous version of EZTouch to install this upgrade. To install:
IMPORTANT! Please read the information below before installing an upgrade. This download will upgrade your existing EZTouch programming software to version 3.0.
Do not delete any existing EZTouch files!! This is a maintenance release, not a full install. You must have a previous version of EZTouch to install this upgrade. To install:
Data
Highway Plus files
This ZIP file contains the released DLL and PLC file for A-B Data Highway Plus
that allows character swapping for strings in the EZTouch panel. This DLL is
released for version 2.4 of EZTouch. The DLL file must be copied to the EZTouch
directory and the PLC file must be copied to the DRIVERS sub-directory
This file is a DEMO project only compatible with the EZ-S8C-F and EZ-T10C-F touch panels. This Demo Project does not require the panel to be connected to a PLC.
Example Program: Setting the PLC Date and Time using the EZTouch Panel
This example has an EZ Touch project and a DirectSoft32 Ladder program that shows how the PLC Clock for the (250,350,440,450 and 05(with optional D0-01MC module installed)) using the DATE and TIME instructions.
NOTE: If you are using the Day of the Week ( V7771 in all CPUs ) ,for any reason, you will not be able to use this example. You will have to set the PLC date and time from DirectSoft