AutomationDirect Logo EZTouch Software Frequently Asked Questions


 

Press "Ctrl-F" to search for specific words in this FAQ.


Click here to view all EZTouch Software FAQs with answers on one page.

  1. Can I change the Data Type of a Tag Name's assigned Address String (PLC Address)?
  2. Can the Tag Database be exported to DirectSOFT32 or other applications?
  3. How do I convert a project from one panel size to another?
  4. Can I use the Power Up Screen selection (under the Project Attributes > General menu) and also use the Switch to Screen Number (under Project Attributes > PLC to Panel)?
  5. Can I place objects anywhere on the screen?
  6. What is a touchcell?
  7. Can I use the floating point data type with all objects?
  8. Why do I not see all the discrete tags in a pushbutton object?
  9. Can I use a label on a vertical radio button?
  10. How does a radio button work?
  11. What is the initial state of objects when the project is written to the panel?
  12. What will be the state of objects if they are mapped to internal tags?
  13. When I select a group of objects and try to move them, all the objects do not move. Why?
  14. When I have objects at the boundary of the screen, I am not able to move the objects freely (vertically up/down or Horizontally left/right near the boundary). What can I do to correct this?
  15. What is the maximum number of screens that a project can have?
  16. What is the maximum number of alarms that a project can have?
  17. What is the maximum number of messages I can have in the Message Database?
  18. Can I insert a 640x480 bitmap on a screen?
  19. Is it possible to find out whether the compressed bitmap size is less than 64K before trying to insert the bitmap?
  20. Is there a limit to the number of objects that can be placed on a single screen?
  21. Is there a demo version of the EZTouch software?
  22. Will a line graph continue to trend if you are not on that screen?
  23. Will any touch panel display info from a 0-20mA device?
  24. Will the EZ-Touch panels be able to communicate to MUSHOSHITO PLCs ?
  25. Does the EZ Touch panel have Boolean Expressions?
  26. Does the EZ Touch panel have an Opto 22 driver?
  27. Will EZ Touch communicate to DSDATA?
  28. Does EZ Touch work with Think N Do 5.2 and earlier versions?
  29. With EZ Touch Editor can you put more than 1 button in the same location?
  30. When I open a project in EZ Touch Edit I cannot see the whole screen and I do not have any scroll bars. What could be wrong?
  31. Can I scale my Numeric Display and Numeric Input Objects in the EZ Touch software?
  32. Will my EZ Touch software work with ThinknDo Studio versions 6.0 and 6.1 ?
  33. Can the EZTouch access the ASCII table in the AB SLC5/03?
  34. What do I need to setup in EZ Touch Edit so I can change screens with my PLC?


Troubleshooting Guides