AutomationDirect Logo EZTouch Panels Frequently Asked Questions


 

Press "Ctrl-F" to search for specific words in this FAQ.

Would you prefer to narrow the list of EZTouch Panels FAQs? Select a category from this list:


Click here to view all EZTouch Panels FAQs with answers on one page.

  1. Does the new EZ-Touch panel have an ASCII driver?
  2. Will the EZ-Touch panels have a driver for SIMAX/SQUARE D?
  3. What agency approvals do the EZTouch panels carry?
  4. What are the PC requirements to be used with the EZTouch panel?
  5. What Serial Drivers does the EZ-S6C-K 6" Color Touch Panel support?
  6. What are the specifications on the communication ports?
  7. How many screens can I have using the EZTouch panel?
  8. Does the EZTouch panel have a built in clock feature?
  9. Does the EZTouch have password protection?
  10. Does the EZTouch panel have serial printer capabilities?
  11. Do the EZTouch panels support Allen Bradley PLC's?
  12. What other PLC's do the EZTouch Panels support?
  13. Does the DL05 & DL06 family of PLC's support the EZTouch panel?
  14. Does the DL-205 family of PLC's support the EZTouch panel?
  15. Does the DL-305 family of PLC's support the EZTouch panel?
  16. Does the DL-405 family of PLC's support the EZTouch panel?
  17. Does the H2-WinPLC support the EZTouch panel?
  18. Do you carry replacement parts and\or accessories for the EZTouch panels?
  19. What are the Vibration specifications for the EZTouch panels?
  20. What is the Electrical Noise Tolerance of the EZTouch panel?
  21. Are any of your EZTouch panels AC powered?
  22. I am unable to communicate with the EZTouch panel from my Programming Computer, what are some things that I can check to ensure that I have a proper set-up?
  23. There is an LED located on the back of my panel, what does the different mode of colors mean?
  24. Does the EZTouch have a built in fuse protection device?
  25. Can I remove the RAM or Flash card while my unit is still powered up?
  26. I have a large project that requires more than the standard 512K of memory. What are my options for additional memory?
  27. Will the EZ Touch be able to display STRING data from Think & Do?
  28. Will the EZ Touch panels be able to communicate to my Servo Drive?
  29. Are the EZ-Touch panels a direct replacement for the Direct Touch Panels?
  30. Do the EZ-Touch panels support the AB Ethernet IP protocol that the Controllogix PLCs use?
  31. If a Flash memory card is installed, does the panel still run off of the RAM?
  32. Will the EZ-Touch panel be a Master or slave when communicating Modbus?
  33. Will the Direct Touch and EZ Touch panels work with the Terminator T1K-RSSS Module?
  34. Do the EZ Touch panels or your PLCs support "Pass Through" functionality so I can download to both by using only one communication port?
  35. Can I connect a GE VersaMax PLC to the EZTouch panel?
  36. Will the EZ-T10C-F work with Modicon?
  37. Is the EZTouch cable the same for all different size panels?
  38. Does the DL105 family of PLC's support the EZTouch panels?
  39. Will using a Stylus (like for a Palm Pilot) damage my EZ Touch display?
  40. Are the EZTouch panels susceptible to image Burn-In, that is if I do not use the screen saver option?
  41. Q: How far can I run a cable from a D2-250 to the EZTouch panel?
  42. Will the communication rate between an EZTouch panel and the PLC slow down as more screens are added to the panel?
  43. I keep getting the error "Protocol Error" on my EZ Touch panel when connected to my Directlogic PLC. The com settings for my PLC port and EZ Touch panel match. What could be wrong?
  44. What type of external Power fuses are recommended for the EZTouch and EZText Panels?
  45. How can I protect my EZTouch project from being copied or altered by others?
  46. Does the EZTouch series have a driver for the Honeywell HC900 controller?
  47. I would like to connect an EZ Touch panel to my Allen Bradley Controllogix PLC. What are my options?
  48. What software version is required for my firmware version?
  49. Do you have an adapter for the D2-DSCBL and EZ-2CBL cables so that I can use them on port 2 of a DL06, DL250-1, or DL260 instead of on port 1? I’m using DirectSoft32 with the RJ-12 PLC connector cable (D2-DSCBL) and/or I’m using an EZ-Text/EZ-Touch panel with the RJ-12 PLC connector (EZ-2CBL) to connect to port 1 of my DL06, DL250-1, or DL260 PLC. I want to connect to port 2 of these processors, which has a 15-pin high density connector.
  50. Where can I get the latest English and Spanish manuals as PDFs?
  51. What do I need to do to replace/upgrade my old EZ Touch panel to a CMore panel?


Troubleshooting Guides