AutomationDirect Technical Support
AutomationDirect | Direct Sales in US and Canada | 1-800-633-0405

ViewMarq Displays Frequently Asked Questions AutomationDirect Logo


Press "Ctrl-F" to search for specific words in this FAQ.


Click here to view all ViewMarq Displays FAQs with answers on one page.

  1. How many colors are displayed by a ViewMarq LED message display?
  2. What are the viewing distances for ViewMarq?
  3. What type of information can ViewMarq display?
  4. What hardware/software is needed to control the messages on the ViewMarq display?
  5. How do I create text messages for ViewMarq?
  6. What size characters can ViewMarq display?
  7. Can ViewMarq display graphics?
  8. Is Ethernet support included?
  9. For the Ethernet connection, do I need a cross-over or patch cable?
  10. Is the ViewMarq display firmware field upgradable?
  11. Which PC operating systems support ViewMarq software?
  12. Is ViewMarq suitable for outdoor use?
  13. Can ViewMarq be used as a standalone product?
  14. Does ViewMarq have a real time clock?
  15. What agency approvals does ViewMarq offer?
  16. Are there mounting limitations for ViewMarq?
  17. What power requirements does ViewMarq have?


Troubleshooting Guides


Copyright © 1999- AutomationDirect.com. ALL RIGHTS RESERVED