AutomationDirect Logo Selector Switch Frequently Asked Questions


Press "Ctrl-F" to search for specific words in this FAQ.


Click here to view all Selector Switch FAQs with answers on one page.

  1. Do you offer a 3 position "spring return" switch?
  2. What is the current draw on the 24 Volt Centsable Incandescent Indicators & Illuminated Switches?
  3. What is the current draw on the 24 Volt Centsable LED Indicators?
  4. What is the current draw on the 120 Volt Centsable Incandescent Indicators & Illuminated Switches?
  5. What is the current draw on the 120 Volt Centsable LED Indicators?
  6. Are your foot switches maintained or momentary?
  7. Can the same Cutler-Hammer selector switch operator be changed to be a 2 position or 3 position unit?


Troubleshooting Guides