AutomationDirect Logo Selector Switches Frequently Asked Questions


« Return to the FAQ index

Question Can the same Cutler-Hammer selector switch operator be changed to be a 2 position or 3 position unit?
Answer Yes. If you remove the knob/lever from the body, there is a plastic piece that interfaces between the knob/lever and the body. It usually sticks into either the knob/lever or body when they are separated, so you will have to physically remove this piece. This piece has a wedge-shaped extrusion that fits into one of three wedge-shaped notches in the body. Each of the wedge-shaped notches in the body piece has a number molded in the notch itself, either 2, 3, or 4. Place the raised notch from the plastic piece into the notch labeled 2 for a 2-position selector switch, or 3 for a 3-position selector switch. Our switches don't use the 4-position option.

FAQ Subcategory:

This item was last updated on 01-22-2009
Document ID: 1123


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.