AutomationDirect Logo Selector Switches Frequently Asked Questions


 

Use "Ctrl-F" to search for specific words in this FAQ.

Question: Do you offer a 3 position "spring return" switch?
Answer: Yes, all of our 3 position switches at this time are available as "spring return" and "maintained" models.
FAQ ID: 344

Question: What is the current draw on the 24 Volt Centsable Incandescent Indicators & Illuminated Switches?
Answer: 83 ma.
FAQ ID: 738

Question: What is the current draw on the 24 Volt Centsable LED Indicators?
Answer: 26 ma.
FAQ ID: 739

Question: What is the current draw on the 120 Volt Centsable Incandescent Indicators & Illuminated Switches?
Answer: 20 ma.
FAQ ID: 740

Question: What is the current draw on the 120 Volt Centsable LED Indicators?
Answer: 5 ma.
FAQ ID: 741

Question: Are your foot switches maintained or momentary?
Answer: All of our foot switches are spring-return to the UP position, where the contacts are at their default state. The are not maintained type pedals. All but the RED unit also include a safety actuating lever which must be pushed in with your foot before you can press down on the pedal.
FAQ ID: 1109

Question: Can the same Cutler-Hammer selector switch operator be changed to be a 2 position or 3 position unit?
Answer: Yes. If you remove the knob/lever from the body, there is a plastic piece that interfaces between the knob/lever and the body. It usually sticks into either the knob/lever or body when they are separated, so you will have to physically remove this piece. This piece has a wedge-shaped extrusion that fits into one of three wedge-shaped notches in the body. Each of the wedge-shaped notches in the body piece has a number molded in the notch itself, either 2, 3, or 4. Place the raised notch from the plastic piece into the notch labeled 2 for a 2-position selector switch, or 3 for a 3-position selector switch. Our switches don't use the 4-position option.
FAQ ID: 1123