AutomationDirect Logo DL305 - All CPUs Frequently Asked Questions


Press "Ctrl-F" to search for specific words in this FAQ.

Would you prefer to narrow the list of DL305 - All CPUs FAQs? Select a category from this list:

Related DL305 FAQ Pages:


Click here to view all DL305 - All CPUs FAQs with answers on one page.

  1. How can I override inputs and outputs in my DL305?
  2. Do you offer a 24 VDC current sinking input module for the DL305?
  3. I am using a 305 system with a LIC and a RIC. Are they compatible with the new "-1" bases?
  4. What is the accuracy of the PLC real-time clock?
  5. What is the torque specification for the terminal blocks on the DL305 modules?
  6. How often should I change the backup battery?
  7. Does the DL305 series support DNP 3.0 protocol?
  8. How would we check this PLC to make sure that it is calibrated?
  9. Does the DL305 series support fiber optic connections?
  10. Do you offer precision resistors?
  11. Are the DL305 bases class1 div2 Canadian rated?
  12. I forgot my password, what are my options?
  13. Are the fuses replaceable on the D3-08TA-2?
  14. Can I buy the DL305 base power supply separate?
  15. Does the D3-232-DCU work with the IC610CPU101 CPU?
  16. What is the SCCR rating for the DL305 PLCs?


Troubleshooting Guides