AutomationDirect Technical Support
AutomationDirect | Direct Sales in US and Canada | 1-800-633-0405

DINnectors Frequently Asked Questions AutomationDirect Logo


Press "Ctrl-F" to search for specific words in this FAQ.


Click here to view all DINnectors FAQs with answers on one page.

  1. Where is the CE Declaration of Conformity for Dinnectors?
  2. What is the screw size that fits the jumper hole in the DN-T12 block?
  3. Do you have any Fuse Terminal Blocks that go up to a 40AMP rating?
  4. What is the UL flammability rating for the plastic on the DINnector blocks?
  5. Will the DN-LT fit the DN-T12?
  6. What is the temperature rating of the M094 terminal blocks?
  7. What is the difference between class CC fuses and Midget fuses for use in fuse blocks and fuse holders?
  8. The blown-fuse LED is not indicating when no fuse is installed in the dinnector?
  9. What does the DIN mean on DIN rails and DINnectors?
  10. Are the BM series insulated wire ferrules UL listed?
  11. What size screws are used in the DN series jumpers?
  12. What was re-designed on the Dinnector Terminal Blocks?
  13. Why are the Dinnector Terminal Blocks being re-designed?
  14. What is the benefit of using the plug in jumpers verse the screw down jumpers system?
  15. Why would I use the DN-J2CUT and DN-J4CUT tool over diagonal cutters or other cutting pliers to cut the insulated plug in jumpers?
  16. What is the temp rating for the BM Direct-mount terminal blocks?
  17. What is the SCCR rating of DINnector terminal blocks?
  18. What is the recommended tightening torque spec for DN-EB35


Troubleshooting Guides


Copyright © 1999- AutomationDirect.com. ALL RIGHTS RESERVED