Use "Ctrl-F" to search for specific words in this FAQ.
| Question: Where is the CE Declaration of Conformity for Dinnectors? |
| Answer: The CE Declaration of Conformity for Dinnectors is on our web site. |
| FAQ ID: 311 |
| Question: What is the screw size that fits the jumper hole in the DN-T12 block? |
| Answer: M 2.6 X 0.45 |
| FAQ ID: 455 |
| Question: Do you have any Fuse Terminal Blocks that go up to a 40AMP rating? |
| Answer: Not at this time, only 30 AMP. |
| FAQ ID: 483 |
| Question: What is the UL flammability rating for the plastic on the DINnector blocks? |
| Answer: It’s rating is: UL94V2 |
| FAQ ID: 484 |
| Question: Will the DN-LT fit the DN-T12? |
| Answer: Yes. |
| FAQ ID: 814 |
| Question: What is the temperature rating of the M094 terminal blocks? |
| Answer: 105C |
| FAQ ID: 849 |
| Question: What is the difference between class CC fuses and Midget fuses for use in DN-FM6 and DN-FM6L fuse terminal blocks? |
| Answer: Class CC fuses are current limiting fuses with rejection tips on the bottoms to prevent them for being used in holders not rated similarly. Midget fuses are defined as supplemental fuses and are not rated for current limiting. They do not have rejection tips because they can be used in most fuse holders regardless of class ratings. Refer to NEC 110-10 for more information on this subject. |
| FAQ ID: 891 |
| Question: The blown-fuse LED is not indicating when no fuse is installed in the dinnector? |
| Answer: Insure that the polarity is correct (I.E. the hinge is on the positive side.) Install fuses and finish the circuit as if ready to operate. When the system is known operational, power down and remove the power side only fuse. The LED should come on when the circuit is complete and has a load. There is a lot of debate over fuse protecting the neutral (grounded conductor/white) conductor of a control circuit. The rule of thumb is to treat as a standard electrical circuit with no fuse on the neutral, only the hot. OPCD's, which open the hot and neutral simultaneously, fall under this category. However, a system with an ungrounded secondary needs to have the neutral fused. If one shorts to ground without it, the system will have a major failure. Refer to NEC articles 240 & 250. |
| FAQ ID: 892 |
| Question: What does the DIN mean on DIN rails and DINnectors? |
| Answer: DIN stands for "Deutsches Institut fur Normung", which means "German Institute for Standardization." In the 1970's the name DIN became the official symbol for technical standardization in Germany. It has become commonplace for Automation equipment to be mounted on 35mm DIN rails. The DIN standard is used for normalization of mounting for everything from plc's to small drives industry wide in North America. |
| FAQ ID: 909 |
| Question: Are the BM series insulated wire ferrules UL listed? |
| Answer: The issue of UL recognition for ferrules typically comes from UL508A companies that inquire whether our ferrules are UL certified or UL recognized. UL has not to our knowledge issued a set of standards related to regulation of wire ferrules for UL508A. Once a stranded wire is inserted into the ferrule and crimped it makes the ferrule an integral part of the wire. It is no different than tinning the wire end with solder. As long as the diameter of the ferrule with the wire inside does not exceed the capacity for the connector it is placed in, the device should be able to pass UL approval. |
| FAQ ID: 1115 |
| Question: What size screws are used in the DN series jumpers? |
Answer:
|
| FAQ ID: 1252 |
| Question: What was re-designed on the Dinnector Terminal Blocks? |
| Answer: The jumpers system was changed from a screw down jumper bar to an insulated plug in jumper system. |
| FAQ ID: 1268 |
| Question: Why are the Dinnector Terminal Blocks being re-designed? |
| Answer: The plug in jumper system offers an insulted jumper. The insulated jumper offers a better method to comply with IEC 60947-1 standard for clearance between conductive parts. The plug in jumpers system is a faster and easier method of installing jumpers. |
| FAQ ID: 1269 |
| Question: What is the benefit of using the plug in jumpers verse the screw down jumpers system? |
| Answer: The plug in jumpers have the ability to be daisy chained by having (2) rows of holes for jumpers in the DN-T12 and DN-T10 series terminal block. |
| FAQ ID: 1270 |
| Question: Why would I use the DN-J2CUT and DN-J4CUT tool over diagonal cutters or other cutting pliers to cut the insulated plug in jumpers? |
| Answer: The DN-J2CUT and DN-J4CUT will allow the insulated plug in jumpers to keep there insulation on the cut edges of the jumpers. Diagonal cutters or any other cutting tools will remove the protective insulation on the jumpers. |
| FAQ ID: 1271 |