SOFTWARE UPDATE NOTIFICATION: Sign up for our software update e-mail notification service to receive word when a new version of CLICK software is available.
Please read this document regarding critical problems with CLICK software versions prior to v1.12. Version 1.12 addresses these issues.
Programming Software v1.12 (37.1 MB)
CLICK Programming Software CLICK Firmware v1.00 v1.00 v1.10 v1.10 v1.11 v1.12 This ZIP file contains CLICK Programming software version 1.12, the Koyo USB-Serial Driver (necessary if you plan to program your CLICK PLC through a USB port using the supported USB cable), and the software installation guide. This download also includes the latest CLICK firmware. Unzip the file to a directory on your computer and run the Install program.
Note: There is no change to the firmware with software version 1.12. Firmware version 1.10 is still the current firmware version.
Minimum System Requirements:
- Windows2000 or XP Personal Computer with a 333 MHz or higher processor (CPU) clock speed recommended; Intel Pentium/Celeron family or AMD K6/Athlon/Duron family, or compatible processor recommended.
Or, Vista Personal Computer with a 800 MHz or higher processor (CPU) clock speed recommended; Intel Pentium/Celeron family or AMD K6/Athlon/Duron family, or compatible processor recommended.- SVGA 1024x768 pixels resolution. (1280x1024 pixels resolution recommended).
- 300MB free hard-disk space.
- RAM: Windows2000 or XP; 128MB free Ram (512MB recommended). Vista; 512MB free Ram (1GB recommended).
- 9-pin Serial Port or USB Port for project transfer to PLC (USB Port communications also requires USB-to-Serial converter).
Note: Programming cable is also required for communications between PC and PLC.
Changes since v1.11:
- When there are three branches in a rung, Coil and/or Box instructions could be energized unexpectedly.
- When two OR circuits were connected to the same vertical line (master line), there was a syntax error. (OR circuit = Two or more Contact instructions are connected in parallel.)
- The syntax error check algorithm was improved to prevent any incorrect ladder programs from downloading into the CLICK PLC.
- The Drum instruction no longer consumes a TD address in the Event Base mode.
Changes since v1.10:
- Added the CLICK Project Loader tool. This tool is available from the Start menu. See the CLICK Project Loader User Guide for details. (This is also available from the Start menu.)
- Added the Override View.
- Added the Exact Match option to the Address Picker, Cross Reference View and Find windows.
- Included the CLICK Hardware user Manual.
- Improved the communication between the CLICK Programming Software and the CLICK PLC. This improvement would reduce the risk of the software crash that some customers had experienced.
- Changed the icons for the interrupt programs.
- Fixed the problem that the CLICK Programming software opened on the Windows with a European language setup didn't accept the comma as the decimal point.
- Fixed the problem that the Timer instruction was set to retain the current timer value and there were 2 contacts in parallel (OR connection) connected to the enable input of the Timer instruction, the Timer was enabled from the beginning even though the both contacts were off.
Changes since v1.00:
- Supported new Analog CPU modules.
- Added the Battery Backup Setup dialog for the Analog CPU modules.
- Added the Calendar/Clock Setup dialog for the Analog CPU modules.
- Added the Com Port 3 Setup dialog for the Analog CPU modules.
- Improved the CPU Built-in I/O Setup dialog to support the Analog CPU modules.
- Added the Text View.
- Added the ASCII data type.
- Supported 2400 and 4800 bps on Com Port 2 and 3.
- Added the new System Data Registers to store the no communication time period on the Com Ports. (SD41, SD51 and SD61).
- Added the two Fill Down buttons to the Drum instruction.
- Improved the Copy instruction (Single Copy mode) to support the Pointer addressing as the Destination parameter.
- Improved the Receive instruction (ASCII mode) to store the length of the received text message.
- Improved the Send instruction (ASCII mode) to embed the ASCII codes and Memory Addresses in the text message.
Please see the Readme.txt file in the download ZIP file for additional information and instructions.