AutomationDirect logo Firmware Revisions for CLICK



Latest shipping version:

 

Recent Firmware History:


Version: V1.10
Details:
[New features]
- Supported the new Analog CPU modules (C0-02DD1-D, C0-02DD2-D and C0-02DR-D)
- Supported the Battery Backup feature for the Analog CPU modules.
- Supported the Calendar/Clock feature for the Analog CPU modules.
- Added the ASCII data type.
- Supported 2400 and 4800 bps on Com Port 2 and 3.
- Added the new System Data Registers to store the no communication time period on the Com Ports. (SD41, SD51 and SD61).
- Improved the Copy instruction (Single Copy mode) to support the Pointer addressing as the Destination parameter.
- Improved the Receive instruction (ASCII mode) to store the length of the received text message.
- Improved the Send instruction (ASCII mode) to embed the ASCII codes and Memory Addresses in the text message.

[Fixed bugs]
- Data registers DS4097-DS4500 and DD1-DD299 could not retain the values when they were set to 'Retentive'.
- When the Drum instruction completed the last step, the outputs assigned for the step were turned off. However, those outputs were turned on again after the enable input for the Drum instruction was turned off and then turned on again.
- When the Copy instruction had DF addresses as the source addresses in the Block Copy mode, the Copy instruction worked in the Fill mode instead of the Block Copy mode.


Version: V1.00
Details:
This is the first release version.