AutomationDirect Technical Support
AutomationDirect | Direct Sales in US and Canada | 1-800-633-0405

IEC Manual Motor Starter Protectors Frequently Asked Questions AutomationDirect Logo


« Return to the list of questions

Question

Can I use a motor starter protector with Variable speed drives and inverters?

Answer

They are only recommended for multiple motor applications from the output of a single drive. The drive handles the aggregate current monitoring, not the individual motor branch current.

NEC article 430 53c “group motor rating” deals with the concept of conventional across the line motor starters and the requirements of short-circuit protection from feeder to motor branch circuit. These guidelines do not mention variable speed drives. The recommendation is always to follow the manufacturer specification. In this case Hitachi recommends J class fuses.

You would never use a MSP, because it is not rated as a SSPD (short circuit protective device) in North America, in place of these J class fuses. There is also no need of an overload on the output side of the drive unless there are multiple motors being used.

Always check with your local inspectors and municipalities before an installation to verify their local requirements which may differ from the National Code.



FAQ Subcategory: None

This item was last updated on 2002-01-22
Document ID: 898


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.


Copyright © 1999- AutomationDirect.com. ALL RIGHTS RESERVED