AutomationDirect Technical Support
AutomationDirect | Direct Sales in US and Canada | 1-800-633-0405

IEC Manual Motor Starter Protectors Frequently Asked Questions AutomationDirect Logo


« Return to the list of questions

Question

What is the minimum cycle time for a starter?

Answer

When the power is stopped to the motor, the field starts to collapse. Remember this takes a certain amount of time. For that very brief moment; there is some CEMF at the motor terminals. Even though it is decaying just like a standard inductive circuit.

Here’s the problem of two short of cycle time. When power is re-applied, the incoming power can actually be out of phase with the collapsing field. The in-rush current can be at twice the LRA (600% FLA on start-up, up to 1200% in this worse case scenario.)

Of course the above example is a worse case scenario, the stress on the windings and the mechanical stresses that can occur out way the benefits of cycling too fast.

You should find out how long the time constant lasts for the particular motor in your project and give it at least 6-10 times the amount.

Refer to NEMA MG-1 defines the open circuit AC time constant.



FAQ Subcategory: None

This item was last updated on 2001-11-20
Document ID: 889


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.


Copyright © 1999- AutomationDirect.com. ALL RIGHTS RESERVED