AutomationDirect Logo General Drives Questions Frequently Asked Questions


« Return to the FAQ index

Question Do I have to use thermistor protection with my motor/drive? Why does the thermistor resistance change from sensor to sensor?
Answer Here in the US, there are no stipulations requiring the use of thermistors (or other temperature sensing devices). People use them as a common sense method of protecting an investment. NEC article 430-32 lists it as one of 4 ways to be compliant. Other mfg's offer it in many forms; thermistor, pyrometer, thermocouple, and RTD. All of these can be used as a temperature measuring/sensing device. The reason that the resistance differs from sensor to sensor is because of the different type of material or different dimensions of the same material being used.

FAQ Subcategory:

This item was last updated on 02-24-2004
Document ID: 870


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.