AutomationDirect Technical Support
AutomationDirect | Direct Sales in US and Canada | 1-800-633-0405

IEC Manual Motor Starter Protectors Frequently Asked Questions AutomationDirect Logo


« Return to the list of questions

Question

What are the differences between the uses of MSPs in USA versus their uses internationally?

Answer

„h MSP¡¦s USA
o Does not meet UL 489
o Cannot be used for stand alone short circuit breaking
o Can be used as ¡§group motor rating¡¨ (UL/CSA)
o NEC 430-53 (sizing guidelines)
o Indicates that a single short circuit protective device can protect several branch circuits.
o If the short circuit current exceeds the withstand rating of the MSP then fuses must be used in series to protect the circuit or the system must be redesigned to accommodate (NEC 110-10).
„h MSP¡¦s international
o IEC 947-4-1
o Recognized as a stand-alone short circuit protecting device.
o Back-up fuses are only required when the fault current exceeds breaking capacity of the MSP.



FAQ Subcategory: None

This item was last updated on 2004-02-18
Document ID: 857


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.


Copyright © 1999- AutomationDirect.com. ALL RIGHTS RESERVED