AutomationDirect Logo General Drives Questions Frequently Asked Questions


« Return to the FAQ index

Question What is the difference between dual voltage and dual wound motor?
Answer Dual voltage is a reference to a motor that can use either of two different voltage levels, usually 230V or 460V. The motor windings have multiple taps, and the connections vary depending on which voltage is used. Dual wound motor refers to two windings in one motor frame, and can be any combination of poles. With the increased amount of copper, the frames are usually twice the size of a standard motor. A dual wound motor can be used in a drive application with one of the windings not hooked up, but we do not recommend this. It is similar to a round rotor motor with the secondary shorted. The insulation properties are not sufficient to handle PWM.

FAQ Subcategory:

This item was last updated on 02-24-2004
Document ID: 816


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.