AutomationDirect Logo DL205 Frequently Asked Questions


« Return to the FAQ index

Question Which DL205 CPUs support the Power Up in Run Mode feature?
Answer Only the D2-230. If you set bit Bit 13 of V-memory 7633, the D2-230 will power-up in Run provided the CPU does not encounter any errors. The D2-250-1 AND D2-260 have a Run/Term/Stop switch. The D2-240 has a Run/Term switch. In the Run position the CPU is forced into the Run mode if no errors are encountered. No changes are allowed by the attached programming/monitoring device. In the Term position, Run, Program and the Test modes are available. Mode and program changes are allowed by the programming/monitoring device. In the Stop position (D2-250-1 and D2-260 only), the CPU is forced into the Stop mode. No changes are allowed by the attached programming/monitoring device.

FAQ Subcategory:

This item was last updated on 01-07-2004
Document ID: 56


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.