AutomationDirect Logo Sensors Frequently Asked Questions


« Return to the FAQ index

Question Can proximity sensors be connected in series?
Answer Yes. The number of proximity sensors connected in series is dependent on the available voltage to energize the PLC input or load. This voltage is calculated as the sum of voltage drops across each sensor subtracted from the available power supply voltage. Let's use as an example three of the AutomationDirect APS24 series 3-wire NPN sensors, where the brown wire is positive, the black wire is the output, and the blue wire is the negative. The load will be a PLC input. By connecting the sensors in series, all of the sensors must be activated in order for the PLC to receive an input signal. Start by connecting the brown wire (BN+) of each sensor in a daisy chain configuration to the positive terminal (+) of a 24 VDC power supply. Next, connect one side of the load (PLC input module) to the first sensors's brown wire (BN+) and the other side to the black wire (BK). Then connect that same sensor's blue wire (BU-) to the second sensor's black wire (BK). Connect the second sensor's blue wire (BU-) to the third sensor's black wire (BK). For the final termination, connect the third sensor's blue wire (BU-) to the negative (-) terminal on the 24 VDC power supply. In the case of a 2-wire sensor using a sinking configuration, connect one side of the load (PLC input) to the positive terminal (+) of a 24 VDC power supply and the other side of the load to the positive (BN+) of the first sensor. Then, connect the negative (BK or BU-) of the first sensor to the positive (BN+) of the adjacent sensor, continuing this patterns as many times as needed, staying within the voltage restrictions previously mentioned.

FAQ Subcategory:

This item was last updated on 12-05-2007
Document ID: 303


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.