| Question | How many poles should the motor have, and how does this relate to the motor's speed? |
| Answer | Using a four-pole motor will work for most applications. Hitachi inverters can be configured to operate motors with 2, 4, 6, or 8 poles. The greater the number of poles, the slower the base motor speed will be, but it will have higher torque at the slower speed. The number of poles that a motor has determines it's speed at a particular frequency. The synchronous speeds for three phase 60 Hz motors are as follows: 2 pole = 3600 rpm; 4 pole = 1800 rpm; 6 pole = 1200 rpm; 8 pole = 900 rpm. |
FAQ Subcategory:
This item was last updated on 09-25-2007
Document ID: 296
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.