| Question | What is the current draw of the Cutler-Hammer Lamps? |
| Answer | Lamps for 22mm Cutler-Hammer Devices 24 Volt @ 14mA LED monoblock 120 Volt @ 14mA LED monoblock 24 VOLT @ 20mA incandescent W1819 120 VOLT @ 20mA incandescent W1121 6 VOLT @ 200mA incandescent ECX1900-5 130 VOLT @ 20mA incandescent ECX1904-5 24 VOLT @ 26mA LED replacement (ECX part numbers) 120 VOLT @ 5mA LED replacement (ECX part numbers) Lamps for 30mm Cutler-Hammer Devices 24 VOLT @ 50mA incandescent HT8BUBLV3 120 VOLT @ 19mA incandescent HT8BULBV7 |
FAQ Subcategory:
This item was last updated on 02-10-2004
Document ID: 226
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.