Point of View Software Frequently Asked Questions
« Return to the list of questions
Question
The value of indirect tags ( @<TagName> ) are not shown in the web thin client application.
Answer
When a screen is saved as HTML, Studio saves a
.TAGL file in the WEB subfolder. This file has
the list of all tags configured in the screen (objects and dynamics). When a screen is opened in the Web Thin
Client browser, the tags listed in the .TAGL are “enabled� for TCP/IP communication with the server station. It provides an optimized communication between the server station and the Web Thin Client
stations.
Therefore, when using indirect tags (@), the tags pointed will not exchange data with the Server,
unless they have been configured in the screen. In other words, the tags that will be pointed in the screen MUST
be configured in any object of the screen to enable the TCP/IP communication for these tags with the server
station.
 Tip: Add a transparent rectangle (no fill and no line) in the screen corner. Apply the Command dynamic to this
rectangle and configure the tags (which can be pointed by indirect tags during the runtime in the Web Thin
Client station) in the Expression field (keep the Tag Name field blank). So, these tags will be added to the
.TAGL file and they will be available for TCP/IP communication with the Server station.
FAQ Subcategory: None
This item was last updated on 2013-11-19
Document ID: 1494
The information provided in the AutomationDirect
knowledge base is provided "as is" without warranty of any
kind. AutomationDirect disclaims all warranties, either
express or implied, including the warranties of
merchantability and fitness for a particular purpose. In no
event shall AutomationDirect or its suppliers be liable
for any damages whatsoever including direct, indirect,
incidental, consequential, loss of business profits or
special damages, even if AutomationDirect or its
suppliers have been advised of the possibility of such
damages. Some states do not allow the exclusion of
limitation of liability for consequential or incidental
damages so the foregoing limitation may not apply.