AutomationDirect Logo SureServo Drives and Motors Frequently Asked Questions


« Return to the FAQ index

Question How do you program the servo for torque control?
Answer The servo drive can receive a +/- 10 Volt analog reference of torque, that you can scale for the proper range between +/- 300%, Set the parameter P1-01 as 3 or 5. Additionally, you can use 3 preset values stored on the specific registers the servo drive and each one of them can be selected with 2 configured digital inputs. Finally, you can send set point of torque though MODBUS communications from a Master that talks MODBUS at rate of up to 115.2 kBaud. More information can be seen on the chapter 5 of the user manual, rev 2/2008. One example can be found on the application note AN-SERV- 002.

FAQ Subcategory:

This item was last updated on 03-05-2009
Document ID: 1153


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.