AutomationDirect Technical Support
AutomationDirect | Direct Sales in US and Canada | 1-800-633-0405

Circuit Protection Frequently Asked Questions AutomationDirect Logo


« Return to the list of questions

Question

How do I get my disconnect switch to close? I rotate the knob on my disconnect switch, but the main contacts do not close.

Answer

The SIRCO and Fuserbloc Series disconnect switches capable of three positions, ONLY when combined with a handle allowing the TEST feature. If the TEST feature is purchased, the disconnect switch has three positions/functions for the actuator as follows:
  • T = Test - Only the auxiliary contact are closed (use for control circuit testing)
  • 0 = Off - Both the auxiliary and main contacts are open
  • 1 = On - Both the auxiliary and main contacts are closed

The sight window indicates the positioning of the actuator.
  • From 0 to T is by CCW Rotation of the Actuator
  • From 0 to 1 is by CW Rotation of the Actuator

Note: The force required for CW rotation is somewhat high. It may feel like the lever may break off, but keep turning until the "1" position indicator appears in the sight window. The Socomec Instruction Sheets may help


FAQ Subcategory: None

This item was last updated on 2022-10-05
Document ID: 1122


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.


Copyright © 1999- AutomationDirect.com. ALL RIGHTS RESERVED