AutomationDirect Logo GS Series Drives Frequently Asked Questions


« Return to the FAQ index

Question Is there a good way to do a master/follower with the VFDs?
Answer Master/follower is a combination of AC drives and motors to get the follower motor to have a proportional speed of the master motor.
The GS2 and GS3 VFD's have an analog output 0-10 Volt for frequency.
This can be used for outputting an approximate speed control signal.
Error can be from 1% to 5 %, depending on the speed percentage; at lower speeds, the error is bigger.
You may offset the input frequency of the follower using the parameters P4-01 to 4-03
Just connect AO of the master into the analog input for frequency set point on the follower with a wire. Connect the ACM terminals from the master to the follower.
Program the analog output for frequency and the analog input for 0 10 Volt (P4-00 as 2)
If you want higher precision, consider the use of Durapulse drives with encoder feedback.
This will reduce the error to less than 0.5%.

In either case, this is not electronic gearing.

FAQ Subcategory:

This item was last updated on 07-28-2009
Document ID: 1076


The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.