| Question | Can the WinPLC be used with an operator interface? |
| Answer | Yes, the C-More and C-More Micro panels have Entivity Modbus drivers. C-More panels can use Modbus RTU(serial) and Modbus TCP/IP(Ethernet). C-More -R panels do not have Ethernet. C-More Micro panels can use Modbus RTU(serial) only. The WinPLC must have Modbus RTU enabled, this is set in the I/O view and is off by default. Both require that the Think and Do project be saved to disk so you can reference the .MAP file for the I/O mapping in the device driver configuration. Note! If you make changes to the WinPLC project you must re-read the .map file for the addresses to be corrected in the panel. Also note that String Tags > S-192 cannot be read from the WinPLC as they do not have Modbus Addresses for tags greater than S-192 |
FAQ Subcategory:
This item was last updated on 08-25-2009
Document ID: 1039
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.