| Question | Do you have an adapter for the D2-DSCBL and EZ-2CBL cables so that I can use them on port 2 of a DL06, DL250-1, or DL260 instead of on port 1? I'm using DirectSoft32 with the RJ-12 PLC connector cable (D2-DSCBL) and/or I'm using an EZ-Text/EZ-Touch panel with the RJ-12 PLC connector (EZ-2CBL) to connect to port 1 of my DL06, DL250-1, or DL260 PLC. I want to connect to port 2 of these processors, which has a 15-pin high density connector. |
| Answer | Yes. In any of the situations listed above, you can use the FA-15HD adapter to connect to port 2 of a DL06, DL250-1, or DL260. The FA-15HD adapter will work with DirectSoft32 and the D2-DSCBL, or with an EZ-Text or EZ-Touch panel and the EZ-2CBL cable to allow them to connect to port 2 of the DL06, DL250-1, or DL260. Since port 2 is configurable on these PLCs, you must make sure the protocol and port settings match on both devices. The FA-15HD adapter can be used with the D2-DSCBL, the EZ-2CBL, or the FA-CABKIT. The FA-15HD adapter can NOT be used with the DV-1000 or the D2-HPP. |
FAQ Subcategory:
This item was last updated on 10-22-2009
Document ID: 1023
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.