| Question | Can GE Series 1/1+ be replaced with a PLC Direct 305 CPU? |
| Answer | Yes, the GE Series 1/1+ can be replaced with the D3-330 or D3-340 CPU. These CPUs are upward compatible from the GE CPUs with the exception of the IC610CPU106 which is the same as the D3-330 CPU. The prom chip from any GE CPU with 3.7K of memory can be transferred to the D3-330 CPU, but not the D3-340. |
FAQ Subcategory:
This item was last updated on 02-09-2004
Document ID: 101
The information provided in the AutomationDirect knowledge base is provided "as is" without warranty of any kind. AutomationDirect disclaims all warranties, either express or implied, including the warranties of merchantability and fitness for a particular purpose. In no event shall AutomationDirect or its suppliers be liable for any damages whatsoever including direct, indirect, incidental, consequential, loss of business profits or special damages, even if AutomationDirect or its suppliers have been advised of the possibility of such damages. Some states do not allow the exclusion of limitation of liability for consequential or incidental damages so the foregoing limitation may not apply.