AutomationDirect LogoDL405 Frequently Asked Questions




Product Selected: DL405
Category Selected: Local and Remote I/O

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: Does the D4-RM have to be at the end of the chain or can it be wired in the chain (i.e., with slaves at each end)?
Answer: The D4-RM does need to be at one end of the physical connection chain. A termination resistor is also required here and at the last slave (which is added by jumpering T to 1).
FAQ ID: 141

Question: Can I run remotes out of sequence, i.e., #1, #3, #6, and #2?
Answer: Although we suggest you to keep in sequence, you are allowed to do this using the D4-450. You will need to address each slave.
FAQ ID: 399

Question: Do you offer a DL405 slice slave that has AC I/O?
Answer: Not at this time.
FAQ ID: 601