AutomationDirect LogoDL405 Frequently Asked Questions




Product Selected: DL405
Category Selected: High-speed count / Pulse out

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: Is there a limitation on the number of High Speed Counters you can install with the DL-430 CPU?
Answer: Yes, the number of High Speed Counters you can install is 8. They cannot be installed in a remote base.
FAQ ID: 138

Question: Can you set up the High Speed Interface Card in a remote unit?
Answer: No, it must be set up in a local base.
FAQ ID: 664

Question: Can the D4-HSC handle differential counting?
Answer: No.
FAQ ID: 704