DL405
Frequently Asked Questions
Product Selected: DL405
Category Selected: Power, I/O, and Wiring
Return to the FAQ index
Press "Ctrl-F" to search for specific words in this FAQ.
| Question: What is the torque specification for the terminal blocks on the DL405 modules?
|
Answer: 0.9 +/- 0.1 Nm (0.062 +/- 0.007 lb-ft)
|
| FAQ ID: 139 |
| Question: What is the current rating on a D4-450DC-1 cpu? |
| Answer: It is 3100ma, same as the AC powered unit. |
| FAQ ID: 152 |
| Question: What is standard current draw on the D4-450 CPU @110VAC? |
| Answer: Approx 0.45 amps. We suggest a 0.75 amp slow blow fuse. |
| FAQ ID: 154 |
| Question: What are the threshold voltages on the D4-HSC? |
| Answer: 4.75 v - on voltage 2 v - off |
| FAQ ID: 156 |
| Question: What is the part # for spare terminal blocks for F4-08TRS-1? |
| Answer: D4-8IOCON. |
| FAQ ID: 333 |
| Question: Can you common the CA and CB on the D4-16ND2F module? |
| Answer: Yes. |
| FAQ ID: 334 |
| Question: Can an I/O connector be connected to a D4-FILL module so wiring for a future module can be in place?
|
Answer: Yes, the D4-FILL does have the retaining nuts in place to attach the I/O connector.
|
| FAQ ID: 400 |
| Question: On the D4-RSDC, Is the power supply isolated from ground or is it floating?
|
Answer: It is isolated with a transformer.
|
| FAQ ID: 599 |
| Question: Q: What is the wire size in the D4-IOCBL-1?
|
| Answer: A: The diameter is 0.38 mm, or slightly smaller than 26 AWG. |
| FAQ ID: 789 |