AutomationDirect LogoDL405 Frequently Asked Questions




Product Selected: DL405
Category Selected: TI405

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: Will the D4-RAM-1 or the D4-UV-1 work with the TI-435?
Answer: Yes, both of these cartridges will work with the TI-435.
FAQ ID: 140

Question: Is the TI-435 the same as the D4-440?
Answer: Yes, the D4-440 is a direct replacement.
FAQ ID: 398

Question: Will TI software work on a D4-440?
Answer: Yes, but we do not support it.
FAQ ID: 629