DL305 - All CPUs
Frequently Asked Questions
Product Selected: DL305 - All CPUs
Category Selected: Power, I/O, and Wiring
Return to the FAQ index
Press "Ctrl-F" to search for specific words in this FAQ.
| Question: Do you offer a 24 VDC current sinking input module for the DL305?
|
| Answer: Yes, you can use either the D3-08NE3 AC/DC Input module, the D3-16NE3 AC/DC Input module or the F3-16ND3F DC Fast Response Input module. |
| FAQ ID: 107 |
| Question: What is the torque specification for the terminal blocks on the DL305 modules?
|
Answer: 0.4-0.5 Nm (0.027-0.034 lb-ft)
|
| FAQ ID: 116 |
| Question: Are the DL305 bases class1 div2 Canadian rated? |
| Answer: Yes, the standard to reference is UL 1604, which is equivalent to CSA-213. So the CUL mark on the DL305 is recognized by CSA |
| FAQ ID: 130 |
| Question: Are the fuses replaceable on the D3-08TA-2?
|
Answer: These fuses are non-replaceable.
|
| FAQ ID: 662 |
| Question: Can I buy the DL305 base power supply separate?
|
Answer: No, it comes installed on the base.
|
| FAQ ID: 703 |