AutomationDirect LogoWinPLC Frequently Asked Questions




Product Selected: WinPLC
Category Selected: CPU & Programming

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: I am having trouble getting the IP address of my WinPLC set up, is there an easy way to do this? Not using Windows Vista
Answer: The latest Netedit3 software can be used to assign IP addresses to WinPLCs.
You just need to be locally connected to the WinPLC, open Netedit, and select the IPX option.
Then change the IP address of the WinPLC to an appropriate address for your network.



NOTE!
This will not work if using Windows Vista.

Vista does not support the IPX protocol.
FAQ ID: 1058