AutomationDirect LogoDL06 Frequently Asked Questions




Product Selected: DL06
Category Selected: Analog

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: Is there an RTD or thermocouple module for the DL06?
Answer: Yes; use F0-04RTD for up to 4 RTDs or the F0-04THM for up to 4 thermocouples.
FAQ ID: 1018

Question: I added analog IO pointer method during online edits. I then wrote to changes to PLC. But my analog IO still does not work, where do I start checking?
Answer: a. Make sure you go to Program Mode, then back to RUN. If you do online edits while in RUN mode, the program mode you get when you WRITE program to PLC is just a Pause mode. You can verify by viewing values in system words (V700, V701, etc) to see if they hold the expected values. If they do not, they will populate with correct values when you power down and then power up or when you go to Program mode and then back to RUN mode.
b. Information on Pointer Method is found in the D0-OPTIONS-M manual for each analog module. Click here for Options Manual.
FAQ ID: 1174