Product Selected: DL06
Category Selected: High-speed count / Pulse out
Return to the FAQ index
Press "Ctrl-F" to search for specific words in this FAQ.
| Question: Can you put an encoder on the DL06? |
| Answer: Yes. This is explained in chapter 3 of the D0-06USER-M. Your 06 must have DC inputs for this function. |
| FAQ ID: 1001 |
| Question: Can the DL06 series support 2 up counters in one of the high speed modes? |
| Answer: Yes, in mode 10 can support 2 single ended up counters, up to 5 KHz. For any application that requires more counters or faster counting rate, use the H0-CTRIO |
| FAQ ID: 1012 |
| Question: Can I configure a DL06 to do high speed counting and generate high speed pulse output? |
| Answer: a. You can do High Speed Inputs or High Speed outputs, but not both. b. Mode 10 allows you to configure two high speed counters, up to 7 KHz. c. Mode 20 allows you to configure a quadrature counter, which allows counting in clockwise and counter clockwise directions (or count up or down), up to 7 KHz. d. Mode 30 allows you to do high speed pulse outputs up to 10 KHz. It supports three profiles: trapezoidal, registration and velocity. e. Click here for Appendix E of DL06 User Manual. |
| FAQ ID: 1175 |