AutomationDirect LogoDL06 Frequently Asked Questions




Product Selected: DL06
Category Selected: Communications

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: Does the DL06 support Modbus protocol?
Answer: The DL06 supports Modbus RTU, not MODBUS ASCII. Port 1 can be a Modbus slave, address 1 only. Port 2 can be a master or slave with user configurable address
FAQ ID: 990

Question: Does the DL06 work with radio communications?
Answer: Yes, on port 2 if you need handshaking.
FAQ ID: 991

Question: Does the DL06 support peer-to-peer communications?
Answer: Yes, the DL06 does support peer-to-peer communications with the H0-ECOM (Ethernet) module.
FAQ ID: 992

Question: To connect a modem with a DL06, do I need to jump RTS and CTS on the PLC side?
Answer: It is case by case. If your modem does not have RTS/CTS control, you need to jumper RTS and CTS on the PLC side. If your modem has RTS/CTS control, you may connect each signal to the modem. Usually, you would jumper RTS/CTS on the PLC side and the modem side and not be concerned about handshaking.
FAQ ID: 993

Question: Can you print from a DL06?
Answer: Yes - ASCII out on a serial printer only
FAQ ID: 994

Question: Can I make 2 D0-06 slaves on a multi drop communicate to each other?
Answer: No, the data must be routed by the master. If you require peer-to-peer communications you need to use the H0-ECOM ethernet module.
FAQ ID: 999

Question: Can port 1 on the DL06 be a master?
Answer: No.
FAQ ID: 1006

Question: Is the Directnet protocol the same between the DL06 and the DL205?
Answer: Yes.
FAQ ID: 1010

Question: Does the DL06 have Ethernet capabilities?
Answer: Yes, Use H0-ECOM
FAQ ID: 1017

Question: Can I read/write data from/to one or more DL PLC? How about to a non DL device?
Answer: a. The DL06 can use port 2 as a master using Direct Net or Modbus RTU.
b. Port 2 supports RS232, and RS422, for both DirectNet and Modbus. RS485 (2-wire)can only be used with Modbus. If you use RS422 or RS485 you can communicate with a network of devices. All devices on the network need to support the protocol the master DL06 port 2 is configured for.
c. If connecting to third party devices, you will use the Modbus RTU protocol. When doing so you will need to convert Modbus addressing to DL octal addressing. To help with this task, we have a Modbus Conversion utility available on our technical support page.
d. Click here to download Modbus Conversion sheet.
e. The DL06 supports two instructions, MRX and MWX, which allow you to address the Modbus addresses directly without the need to convert to octal addressing.
f. Chapter 4 of the D0-06USER-M manual covers the communications port and networking starting on page 7. Click here for Chapter 4 of DL06 User Manual.
FAQ ID: 1177

Question: What protocol can be used with the RS-485 ( 2-wire) configuration for port 2?
Answer: Modbus is the only protocol that can be used with RS-485. DirectNet and K-Seq are for use with RS-422 (4-wire).
FAQ ID: 1185