AutomationDirect LogoDL06 Frequently Asked Questions




Product Selected: DL06
Category Selected: CPU & Programming

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: Is there a way to detect a low battery condition in the DL-06 PLC?
Answer: Yes, use Special Relay SP43.
FAQ ID: 936

Question: What is the accuracy of the PLC DL06 real-time clock?
Answer: It is +/- 1 minute per month.
FAQ ID: 989

Question: Will my D2-HPP work with the DL06 PLC?
Answer: Yes, but it must have V2.2 or later firmware. However, not all commands are supported.
FAQ ID: 995

Question: Can the DL06 handle larger preset values than 9999 for counts?
Answer: Sure, just use UDC counters that counts up to 99999999.
FAQ ID: 998

Question: I forgot my password, what are my options?
Answer: - Once you have contacted Tech Support, someone will request that you send in your CPU to his or her attention. The program inside the CPU will be lost and irretrievable when we clear the password.
FAQ ID: 1003

Question: What configuration software is necessary to use for DL06?
Answer: You can use the full blown package PC-PGMSW that allows you to program all the ADC PLC families or a subset (PC-PGM-BRICK) that allows you to program the PLC’s DL05, DL105 and DL06. Version 4.0 or higher must be used. Older versions do not support the DL06.
FAQ ID: 1004

Question: Do you offer a memory cartridge for the DL06 family?
Answer: No, we do not.
FAQ ID: 1005

Question: Is there a calendar and date in the DL06?
Answer: Yes. The PLC DL06 has a real time clock that contains the year, month, day of week, day of month, hour, minutes and seconds. The precision is +/-1 minute per month.
FAQ ID: 1008

Question: Does the DL06 have floating point math capabilities?
Answer: Yes.
FAQ ID: 1009

Question: Where are the Hours, Minutes & Seconds stored at using a DL06?
Answer: Hours in V7770; minutes in V7767 and seconds in V7766
FAQ ID: 1011

Question: I just installed a new module in one of the expansion slots but I cannot see it in Configure I/O, what could cause this?
Answer: a. This is most likely the PLC firmware version. You will need to update it.
b. Click here for Koyo Support Tool download..
c. Click here for DL06 firmware download.
d. Install the Koyo Firmware Update Tool and follow the wizard to update the firmware in your PLC.
e. Once updated, check Configure I/O. The module should now be recognized by PLC.
FAQ ID: 1179

Question: Which formula do I use to scale an analog input if my engineering unit does not start at 0?
Answer: Click here for scaling formula.

a. When using BCD or Binary data types, you will lose resolution since you cannot use the fractional values. You can multiply the engineering min and max values by a factor of 10 or 100 to accommodate for this to a certain extent. For example, if your engineering range is 0 to 100, use 0 to 10000.
b. If you are dealing with negative values in DirectLogic PLCs, it will be easier if you use floating point data type.
c. Ladder example using IBOX to scale -10 deg C to 60 deg C, where V2000 is the raw count (0 to 4095):

Click here for scaling example using IBOXs.
FAQ ID: 1182

Question: How do I get the absolute value of a 2s complement negative number so that I can use it as a REAL value?
Answer: a. It is not possible to convert a 2s complement negative number directly to a REAL value.
b. Example 1 below uses V2000 as the 2s complement data source and V3000 as our converted REAL value destination.
i. When a 2s complement value is negative, the most significant bit of the word will be turned on. Therefore, we check to see if V2000 is greater than hex 8000.
ii. If the value in V2000 is less than hex 8000, the value is positive and we can convert using BTOR directly. (Rung 1)
iii. If the value in V2000 is negative, we invert the bit pattern, add 1 to it and store 16 bit result in V3002. We then convert the positive value in V3002 to REAL, multiply it by -1 and store the result in V3000.
Click here for 2s complement ladder Example 1.

c. Example 2 below uses V2000 as the 2s complement data source and V2500 as our converted REAL value destination.
i. When a 2s complement value is negative, the most significant bit of the word will be turned on. In this example we use the actual most significant bit (B2000.15) to determine if value in V2000 is positive or negative.
ii. If the value in V2000 is positive, we convert to REAL using BTOR directly. (Rung 3)
iii. If the value in V2000 is negative, we invert the bit pattern, ANDD the inverted value with KFFFF, add 1 to it, convert the positive value to REAL using BTOR, multiply by -1 and store the result in V2500.
iv. It is important to note that we did not have to store the positive result in an intermediate address in this example. The result of the INV instructions is a 32 bit word stored to the accumulator. Since, we are only dealing with a 16 bit word, we need to mask (get rid of) the most significant 16 bits. To do this we use the ANDD with a value of KFFFF, which turns on only the bottom 16 bits of a 32 bit pattern.
Click here for 2s complement ladder Example 2.
FAQ ID: 1183

Question: Can I change the backup battery with power applied to my DL06 CPU?
Answer: Yes. Open the battery cover on the top right corner of the unit and insert a new battery.
FAQ ID: 1203