AutomationDirect LogoDL205 Frequently Asked Questions




Product Selected: DL205
Category Selected: Analog

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: Is Pointer addressing prohibited for analog modules located in Remote bases?
Answer: Yes - you cannot use the pointer method in remote bases that have analog cards.

FAQ ID: 66

Question: Can you use an F2-04THM and another analog module in a local DL-205 PLC system?
Answer: Yes.
FAQ ID: 85

Question: Is the analog setup for D2-250, D2-250-1 or D2-260 pointer method the same as for D2-240?
Answer: Yes.
FAQ ID: 86

Question: Does your line of EBCs support thermocouple input modules?
Answer: Yes.
FAQ ID: 592

Question: Is a D2-230 capable of analog inputs?
Answer: A: Yes you may use analog inputs with the D2-230.
FAQ ID: 787