AutomationDirect LogoDL205 Frequently Asked Questions




Product Selected: DL205
Category Selected: Communications

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: Can the DL205 communicate to the DL305 or DL405 CPU's?
Answer: Yes, the DL205 CPU's can communicate with the DL305 and DL405 CPU's. The D2-230 can be a slave using the D2-DCM (Data Communications Module). The D2-240 can be a master/slave by using the D2-DCM or the H2-ECOM(-F) (Ethernet Communication Module). Also, the D2-240 can be a slave by using the bottom port on the CPU. The D2-250-1 and D2-260 can be a master/slave by using either the D2-DCM, the bottom port on the CPU or the H2-ECOM(-F).

FAQ ID: 55

Question: Which DL205 CPUs support the H2-ECOM in their base?
Answer: The D2-240,D2-250 and D2-60. The D2-230 does not support the H2-ECOM.
FAQ ID: 58

Question: Can the DL205 be used on a Modbus network?
Answer: The D2-240, D2-250-1 and D2-260 can be used on a Modbus network. The D2-250-1 and D2-260's bottom port can be set to Modbus master/slave. Also, the DCM module can act as a Modbus slave when used with the D2-240 or D2-250 or D2-250-1 or D2-260. The Modbus RTU (hex) protocol is supported.

The D2-230 cannot be used on a Modbus network.
FAQ ID: 62

Question: Does the DL250 bottom port (port 2) support 2 wire + ground (RS-485) networks?
Answer: No, the bottom port of the D2-250 does not support 2 wires + ground (RS-485) networks.
FAQ ID: 67

Question: Where can I find information on how to connect 205 I/O to a 405 master?
Answer: You will need to look at the D4-REMIO-M manual. There are no differences in the 205 and 405 remote; the setup is almost identical.
FAQ ID: 68

Question: Does the DL205 series support DNP 3.0 protocol?
Answer: At this time, it does not.
FAQ ID: 71

Question: How do I write ASCII code for inverter to comm port on a D2-240?
Answer: You cannot; we do not support ASCII in from the CPU except with a D2-260. Use a D2-260 or a F2-CP128.

FAQ ID: 77

Question: Can I use a modem to bottom port of D2-250-1 using K-seq?
Answer: Yes, set the port parity to None or Even.
FAQ ID: 81

Question: What do I need to read a barcode input?
Answer: Use a DL205 with an F2-CP128 module. The other option is to use a D2-260 CPU, which supports ASCII in on port 2. Barcoder scanners are typically ASCII out with 232 comm.
FAQ ID: 82

Question: Can a D2-240 do ASCII in and out?
Answer: No, you must use an F2-CP128 for this case or a D2-260 CPU
FAQ ID: 84

Question: Will the H2-ECOM-F work with the D2-CTRINT?
Answer: Yes.
FAQ ID: 88

Question: Do you offer precision resistors?
Answer: At this time we do not.
FAQ ID: 89

Question: Can the D2-240 and D2-250 do Directnet?
Answer: Yes on both ports, top ports are 9600 baud only though.
FAQ ID: 91

Question: Using a D2-250, can you access a V memory through modbus?
Answer: Yes. There is a section in manual on pg. 4-20 that gives the equivalent.
FAQ ID: 94

Question: Can the DL205 family communicate via Ethernet?
Answer: Yes, you will need a H2-ECOM for this. Exception is the D2-230 CPU.
FAQ ID: 321

Question: What type connectors are on the H2-ECOM?
Answer: Ethernet = RJ-45
FAQ ID: 325

Question: Do we have Profibus protocol in the DL205?
Answer: Yes. We offer the H2-PBC Profibus Slave Base Controller. You can view the H2-PBC-M manual in the documentation section for details. This unit operates as a slave only and replaces the CPU in the DL205 rack.
FAQ ID: 326

Question: Will F2-DEVNET support the AB PLC?
Answer: Yes.
FAQ ID: 328

Question: Can you configure a D2-250-1 port for remote I/O and other protocols at the same time?
Answer: No, when configured for remote I/O, it is dedicated to remote I/O.
FAQ ID: 386

Question: Will the Dsdata server link to the H2-EBC base controller?
Answer: Not directly. The DSData Server can link to PLC CPU's. If the PLC has an ERM connected to an EBC, then DSDAta could get data derived from modules in the EBC rack.
FAQ ID: 389

Question: Can you do 2 way ASCII on port 2 of the D2-250-1?
Answer: No. The 250-1 only supports ASCII OUT on Port 2. The DL06 and DL260 support ASCII IN/OUT on Port 2.
FAQ ID: 390

Question: Will the F2-UNICON support the D2-240?
Answer: Yes, using the bottom port.
FAQ ID: 464

Question: Does the H2-ECOM module have SNMP support?
Answer: No. It only supports TCP/IP and IPX/SPX.
FAQ ID: 468

Question: What is the smallest PLC that has Ethernet capability?
Answer: A D0-05 CPU with an H0-ECOM module. D0-06 and CPUs D2-240, D2-250-1, D2-260 and D4-440 and D4-450 are also capable of Ethernet communication using the appropriate Hx-ECOM module.
FAQ ID: 556

Question: Do we have any examples of how to connect a D2-250-1 or D2-260 to a printer?
Answer: Yes, on the web it is on our Tech Support page at
Technical and Application Notes -> PLC HGardware: Communications -> AN-D05-001.
This example is for a DL05 PLC, but it will work for a D2-250-1 or D2-260 CPU as well.
FAQ ID: 591

Question: Will the ISONET work with bottom port of the D2-240?
Answer: Yes.

FAQ ID: 596

Question: Using my laptop, Im having trouble linking up to port 2 on the D2-240 / D2-250-1 / D2-260 PLC. Where can I start trouble-shooting?
Answer: Start by trying Port 1 of the PLC. It has a fixed setup scheme and should be easier to troubleshoot. Once connected through Port 1, you can check the configuration of Port 2.
FAQ ID: 626

Question: Will the D2-DCM function in an EBC base?
Answer: Not at this time.
FAQ ID: 654

Question: Does the D2-250 have ASCII in capabilities?
Answer: No it does not. The D2-250-1 has ASCII OUT, and the D2-260 has ASCII IN/OUT.
FAQ ID: 658

Question: Can any ADC products communicate with Modbus Plus?
Answer: No.
FAQ ID: 696

Question: Will the H2-ECOM support peer-to-peer communications?
Answer: Yes.
FAQ ID: 699

Question: Can I use a modem to top port of a D2-250-1?
Answer: Yes, but you need a modem that can be configured to use odd parity.
FAQ ID: 806

Question: Is it possible to use the H0/H2/H4-ECOMS Ethernet modules with Routers on a network.
Answer: In general, assuming you only have a router or gateway, you need only give the ECOM an IP address that is valid on the remote side of the router. Sometimes you need to create a mapping in the router itself that allows IP traffic through the router to the ECOMs IP address, sometimes you need to specify the port number (0x7070), most of the times not.
Then, in DirectSOFT, when you create the link, you specify the ECOM’s IP address, then your PC uses it’s IP address, it’s Netmask and the ECOM’s IP address to determine that the ECOM is not on the local network, and it the goes to the Gateway to see if it can find the ECOM’s IP address, which it can.
But let me stress that this process is most likely going to be different everywhere you try it. If you have a Proxy Server with the Gateway, you’ll likely make a UDP mapping in the Proxy Server software to allow the traffic through. And each proxy software server package is going to be different.
It can be done, but the specific information on how to do it will vary with each particular situation. You will need to get the person who manages the network at each site to figure out how his/her network must be configured to allow this to work.
FAQ ID: 903

Question: What port is used for Modbus TCP for the ECOM100 modules?
Answer: The ECOM100 has port 502 set by default, it can only be changed if the ECOM100 is used as Client(master).
FAQ ID: 1189