Product Selected: DL305 - TI305/GE Series1
Category Selected: CPU & Programming
Return to the FAQ index
Press "Ctrl-F" to search for specific words in this FAQ.
| Question: Can GE Series 1/1+ be replaced with a PLC Direct 305 CPU? |
| Answer: Yes, the GE Series 1/1+ can be replaced with the D3-330 or D3-340 CPU. These CPUs are upward compatible from the GE CPUs with the exception of the IC610CPU106 which is the same as the D3-330 CPU. The prom chip from any GE CPU with 3.7K of memory can be transferred to the D3-330 CPU, but not the D3-340. |
| FAQ ID: 101 |
| Question: Are the TI-305/Series 1 UVPROMs compatible with the D3-330/D3-340 CPUs? |
| Answer: No, the memory sizes are different. They changed early on from 0.7k to 1.7k, then to 3.7k for the D3-330/D3-340. |
| FAQ ID: 108 |
| Question: I would like to replace my GE Series 1 Jr. with a DL305 CPU. How do I retrieve the program and then transfer it? |
| Answer: It is done by cassette recorder and explained in Chapter 5 of the D3-HP-M manual. This may also be found on our web site at D3-HP-M manual. |
| FAQ ID: 113 |
| Question: Will your D3-D4-BAT battery work in the old GE Fanuc Series One CPU? |
| Answer: Yes, those batteries will work. |
| FAQ ID: 114 |
| Question: Can the D3-HP be used with a GE series one CPU? |
| Answer: Yes, as long as the CPU part number begins with IC610. |
| FAQ ID: 126 |
| Question: Will GE 9030CPU work on DL305 system? |
| Answer: No |
| FAQ ID: 128 |
| Question: Will TI Soft support your DL305 hardware? |
| Answer: TI Soft will work with the D3-330 and D3-340 CPUs. It will not work with the D3-350 CPU. |
| FAQ ID: 598 |
| Question: Will the EEprom on an IC610CPU101C interchange with the D3-330 CPU? |
| Answer: No, they are not interchangeable. |
| FAQ ID: 701 |