Product Selected: DL305 - DL350 CPU
Category Selected: CPU & Programming
Return to the FAQ index
Press "Ctrl-F" to search for specific words in this FAQ.
| Question: I'm doing REAL number math and OUTing the value to a register with my D3-350. When I need that number it does not display correctly. What's wrong? |
| Answer: The REAL number PLC's use the IEEE 32 bit floating point format. You must use an OUTD to store the result of a REAL number math operation into V-memory. |
| FAQ ID: 97 |
| Question: I'm upgrading my old DL305 systems to the new D3-350. How will my programs be handled? |
| Answer: The D3-330 and D3-340 use the old 305 instruction set. This is early to mid-80's technology. The new D3-350 uses the new 205/405 memory mapping and instruction set. Unfortunately the only way to convert is to rewrite the program. PLC Direct technical support does not offer this service but we can refer you to integrators who can rewrite your code if you do not wish to do it yourself. |
| FAQ ID: 99 |
| Question: Can you use an OP-CCBL to program a D3-350 CPU? |
| Answer: No...6;2-1 are jumpered together. |
| FAQ ID: 121 |
| Question: Can I force I/O points in the D3-350? |
| Answer: I/O points in the D3-350 firmware version 1.15 or newer can be "forced" using bit override. |
| FAQ ID: 124 |
| Question: What modules does the D3-350 not support? |
| Answer: D3-HSC, D3-232-DCU, D3-422-DCU, D3-HP, D3-HPP, F3-AB64, F3-AB64-R, F3-AB64-T, F3-AB128, F3-AB128-R, F3-AB128-T |
| FAQ ID: 352 |
| Question: Where can I obtain the most current firmware for my CPU? |
| Answer: Go to the following links on our website to check for availability of firmware. Technical Support / Firmware Upgrades / Firmware Only. |
| FAQ ID: 395 |