AutomationDirect LogoDL305 - DL330/340 CPUs Frequently Asked Questions




Product Selected: DL305 - DL330/340 CPUs
Category Selected: CPU & Programming

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: I can't edit control relays from data view with a D3-330 or D3-340. What am I doing wrong?
Answer: You're not doing anything wrong. The D3-330 and D3-340 use Direct Net protocol only. You can only write at a byte level with DirectNet. You must edit the entire R register containing the C bit you wish to change. You should examine the R register containing the C bit and edit the entire register with the BCD value that would reflect the bit pattern you're wanting. The D3-350 also uses DirectNet and you can do the same thing editing V-memory. Better yet, with the D3-350 you can switch to K-Sequence protocol and do bit level reads and writes.
FAQ ID: 98

Question: Do I have to use Stage programming in D3-330P?
Answer: Yes, you have to have at least one stage; i.e. ISG 0.
FAQ ID: 103

Question: Which special relay do I use for "always on" with a D3-330 or D3-340?
Answer: Use STR NOT C374, being C374 one internal relay that closes only on the fist CPU scan. This will be on for all scans except first scan. If you also need first scan, use STR NOT C374 OR STR C374.
FAQ ID: 104

Question: Some of the counters and timers are not working in my D3-330 or D3-340. What's wrong?
Answer: This may be the result of using timers and counters with the same number. For example, Timer 600 and Counter 600. The timers and counters share the same memory area in a D3-330/D3-340 CPU. You cannot use the same number for both a timer and a counter.
FAQ ID: 106

Question: The battery LED is illuminated on by DL305. How do I replace the battery without losing the program?
Answer: You should always make a backup copy of the program using either the Handheld programmer with a cassete tape or using DirectSOFT with a DCU (Data Communications Unit) if at all possible. Then, power down the DL305, remove the old battery and install a new battery (D3-D4-BAT). The memory is capacitor backed and will last several minutes allowing time to replace the old battery.


FAQ ID: 109

Question: Can I do "online edits" to D3-330 or D3-340 CPUs?
Answer: No.
FAQ ID: 122

Question: Q: Can I use the D2-DSCBL with a D3-340?
Answer: A: No; use instead the cable D3-DSCBL-1
FAQ ID: 788