AutomationDirect LogoTerminator I/O Frequently Asked Questions




Product Selected: Terminator I/O
Category Selected: Base Controllers

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: What are the specifications for the T1K-DEVNETS module?
Answer: Those specifications can be found at this link.
FAQ ID: 488

Question: What are the specifications for the T1H-EBC module?
Answer: The specifications can be found at this link.
FAQ ID: 503

Question: What are the specifications for the T1K-RSSS module?
Answer: The specifications can be found at this link.
FAQ ID: 506

Question: What are the specifications for the T1H-PBC module?
Answer: The specifications can be found at this link.
FAQ ID: 507

Question: What are the specifications for the T1K-MODBUS module?
Answer: The specifications can be found at this link.
FAQ ID: 508

Question: Can I use a Terminator EBC from a 405 ECOM?
Answer: This will not work. The ECOM will not work as a master. The Terminator EBC must be used with PC control.
FAQ ID: 602

Question: What version of Think & Do supports Terminator I/O?
Answer: 6.0
FAQ ID: 622