Product Selected: DL105
Category Selected: CPU & Programming
Return to the FAQ index
Press "Ctrl-F" to search for specific words in this FAQ.
| Question: How do I reset my processor back to factory defaults? |
| Answer: Resetting the processor to factory defaults is a two step process. First clear the processor memory by PLC>CLEAR PLC MEMORY. Next initialize the scratchpad by PLC>SETUP>INITIALIZE SCRATCHPAD. Be aware that initializing the scratchpad will reset the system V-memory to defaults. System V-memory contains parameters such as retentive ranges, DV-1000 setup parameters, etc. |
| FAQ ID: 30 |
| Question: My inputs X0-X3 and/or my outputs Y0-Y1 are not working. What's wrong? |
| Answer: The PLC is most likely in a high speed counter mode. When in high speed counter mode inputs X0-X3 and/or Y0-Y1 will not act as normal I/O. To reset the processor to treat X0-X3 and Y0-Y1 as normal I/O, go to PLC>SETUP>INITIALIZE SCRATCHPAD. |
| FAQ ID: 31 |
| Question: How can I override inputs and outputs in my DL105? |
| Answer: The F1-130 does not support override. You can turn bits on or off with Data View for a single scan to trigger events, but the PLC will update the image register on the next scan. The inputs will reflect their actual state and the outputs will be the result of the rung that controls them. You can control outputs by loading a program that consists of an END statement only. From DEBUG>DATA VIEW>NEW/OPEN you can then select the particular bit and use the on/off button to control the element. You can not control inputs. |
| FAQ ID: 32 |
| Question: The run indicator on the CPU is flashing. What's wrong? |
| Answer: The CPU has gone into update mode. This can be caused by an electrical spike to the incoming power or through the relay output if powering an inductive load without using proper surge suppression. To correct this problem, you will need a firmware upgrade and adding surge suppression is recommended. If you prefer to do the upgrade (using your PC), contact technical support for more information. If you do not want to do the upgrade, call for a return authorization number. |
| FAQ ID: 33 |
| Question: Can additional I/O be added to the DL105? |
| Answer: No, the F1-130 is fixed I/O with 10 inputs and 8 outputs. If you require more I/O points, check our DL205 modular PLC system. |
| FAQ ID: 35 |
| Question: My DL105 drops out of run mode intermittently. What's wrong? |
| Answer: This problem occurs only with the relay output version of the DL105. If the relay is driving an inductive load, the load needs to be suppressed using any MOV or TVS. This prevents EMF (noise) from traveling back to the relay and will keep the DL105 from dropping out of run mode. |
| FAQ ID: 38 |
| Question: How long will the DL105 retain its memory while powered down? |
| Answer: The ladder logic is written to EEPROM, which is non-volatile. The V-memory is backed by a super capacitor that will last approximately one week. |
| FAQ ID: 39 |
| Question: What is the accuracy of the PLC real-time clock? |
| Answer: The DL105 has no clock/calendar feature |
| FAQ ID: 41 |
| Question: What is the accuracy of the timer instructions? |
| Answer: The accuracy of the timer instruction is the same as the accuracy of the clock generator used for the microprocessor in the DL105. The accuracy of the clock generator is ± 50 PPM. So the accuracy of the timer instruction is: ±50 PPM * 60 sec * 60 min * 24 hr = ±4.32 seconds (per day) |
| FAQ ID: 42 |
| Question: Are there any plans to CE List or Recognize the DL105? |
| Answer: At this time, there are no plans to CE List this product line. |
| FAQ ID: 43 |
| Question: How would we check this PLC to make sure that it is calibrated? |
| Answer: Our PLCs do not require calibration. |
| FAQ ID: 45 |
| Question: Is there a force option in the DL105? |
| Answer: Not at this time. |
| FAQ ID: 48 |
| Question: Does the DL105 CPU support SBR instruction?? |
| Answer: No. |
| FAQ ID: 320 |
| Question: I forgot my password, what are my options? |
| Answer: Once you have contacted Tech Support, someone will request that you send in your CPU to his or her attention. Always remember to save your program before sending in your unit. The program inside the CPU will be lost and irretrievable when we clear the password. |
| FAQ ID: 384 |
| Question: Where can I obtain the most current firmware for my CPU? |
| Answer: Go to the following links on our website to check for availability of firmware. Technical Support / Firmware Upgrades / Firmware Only. |
| FAQ ID: 385 |
| Question: Does the DL105 have UL approval? |
| Answer: Yes, both UL and CUL. |
| FAQ ID: 650 |
| Question: Q: What type of memory is in the DL105? |
| Answer: A: The RLL program is stored in EEPROM Non-volatile memory. There is no battery backup. |
| FAQ ID: 783 |