AutomationDirect LogoDL05 Frequently Asked Questions




Product Selected: DL05
Category Selected: High-speed count / Pulse out

Return to the FAQ index

Press "Ctrl-F" to search for specific words in this FAQ.

Question: Does the DL05 accept encoder input?
Answer: Yes, the DL05 units with DC inputs will accept encoders. This is explained in chapter 3 of the D0-USER-M. There is also an H0-CTRIO high-speed counter interface module for use in the option slot of the DL05 unit.
FAQ ID: 378

Question: Can the DL05 series support 2 up counters in one of the high speed modes?
Answer: No, only one in mode 10
FAQ ID: 646

Question: Can I drive a stepper motor with a DL05?
Answer: Yes, you can. The instructions are explained in the manual.
FAQ ID: 647

Question: Can I configure a DL05 to do high speed counting and generate high speed pulse output?
Answer: a. You can do High Speed Inputs or High Speed outputs, but not both.
b. Mode 10 allows you to configure one high speed counter, up to 5 KHz.
c. Mode 20 allows you to configure one quadrature counter, which allows counting in clockwise and counter clockwise directions (count up or count down), up to 5 KHz.
d. Mode 30 allows you to do high speed pulse outputs up to 7 KHz. It supports three profiles: trapezoidal, registration and velocity.
e. Click here for Chapter 3 of DL05 User manual.
FAQ ID: 1164