Product Selected: DL05
Category Selected: I/O Modules
Return to the FAQ index
Press "Ctrl-F" to search for specific words in this FAQ.
| Question: What is the I/O addressing of an option card? |
| Answer: An input card will have X100 as the first input point and so on. An output card will have Y100 as the first output and so on. |
| FAQ ID: 1015 |
| Question: Outputs are not turning on in an option module. What could cause this? |
| Answer: a. First input of an optional input module starts at X100. First output of an optional output module starts at Y100. b. OPTIONS manual page 2-15 covers optional module IO mapping. Click here for Chapter 2. c. You can also get information under PLC/Configure IO. Look in the slot under the Address In and Address Out column for starting address. d. Combo modules require more information found in Options manual. D0-OPTIONS-M. Click here for Options Manual. |
| FAQ ID: 1161 |