AutomationDirect Technical Support
AutomationDirect | Direct Sales in US and Canada | 1-800-633-0405

PPC5 Controller Support Resources AutomationDirect Logo


PPC5 Controller Software Download

Configuration Software for ProSense PPC5 Advanced Process Controllers

View End User License Agreement

Download Configuration Software (Current version: R6.02.02)

Release Notes: AutomationDirect.com Initial Release (R6.02.02)

Notes

  • The installation download will install both the "Setting Tool" and a "Network Profile Tool" applications. The "Setting Tool" application is used to configure the PPC5 and the "Network Profile Tool" application is not used with the PPC5 controller series and is not supported by AutomationDirect.com.
  • A USB driver may be required and is included in download above.
  • The Parameter Setting Software uses .Net Framework 4.
  • In order to install the Parameter Setting Software an internet connection is required

Sample PLC Programs

Download sample PLC programs for AutomationDirect PLCs:

  • ProSense PPC5 PLC programs

Copyright © 1999- AutomationDirect.com. ALL RIGHTS RESERVED