Latest shipping version:
Recent Firmware History:
Version: 1.06.02
Details:
(1) Corrected Torque Control by Analog Input to allow 0 to 100% operation.
(2) Improved DI Input operation. When two DIs are set to options 24 & 25 (FWD Jog and REV Jog respectively), and P02.00 is in option 2, 3,
5 or 6, the jog function will ignore direction input from DI2
Version: 1.06.01
Details:
Changed default value of P09.94 to 1
Version: 1.06
Details:
(1) Corrected handling of CP32 error
(2) Corrected OT1 Over Torque error not resetting
(3) Add Ethernet comm card setting of 6006h Torque Command. P11.34 value
Version: 1.05
Details:
(1) Added support for GS20A-CM-EIP2
(2) Added Gsoft2 connectivity through Ethernet card support
Version: 1.04
Details:
VERSION NUMBER
RELEASE DATE
09/01/2024
DETAILS
(1) Parameters P01.12, P01.13, P01.14, P01.15, P01.16, P01.17, P01.18, P01.19, P08.04,
P08.05, P08.66, will save to EEPROM on power loss.
Version: 1.04
Details:
VERSION NUMBER
RELEASE DATE
09/01/2024
DETAILS
(1) Parameters P01.12, P01.13, P01.14, P01.15, P01.16, P01.17, P01.18, P01.19, P08.04,
P08.05, P08.66, will save to EEPROM on power loss.
Version: 1.03.0
Details:
VERSION NUMBER
1.03.0
RELEASE DATE
21/08/2023
DETAILS
V1.03.0 (P00.06)
Date Code 23285 (P00.50)
(1) Changed P00.21, P02.00, P02.03, P02.04 and P02.13 to allow for 2 wire jog reverse.
(2) Changed attributes for P03.58, P03.60 and P03.62 to allow -100%.
(3) Change to allow P11.33 to be set to 5 Comm Card.
(4) Changed P05.29 to be kW-Hour.
(5) Changed P05.26, P05.27 And P05.28 to reflect low power output drives.
(6) Change to value in Modbus register 210Fh. Value will be one decimal place when the value in 2114h is 1, and
two decimal places when the value in 2114h is 2.
(7) This firmware will require the use of the EDS file version 1.2 or greater, AOI file version 1.4 or higher.
(8) This firmware will require the use of Gsoft2, Version 2.0.2.0 or higher.
Version: 1.02.0
Details:
V1.02.0 (P00.06)
Date Code 22342 (P00.50)
(1) Changed P07.20 decelerate behavior.
(2) P06.13, P06.27, P14.80, P14.82 default value set to 1 for Electronic Thermal overload.
(3) Corrected TQC Sensorless torque limits in torque mode.
(4) Corrected GS2 mode - MI 99 allow for duplicate setting for digital updates.
Version: 1.01.0
Details:
V1.01.0 (P00.06)
Date Code 21355 (P00.50)
(1) Modified the display of motor speed to correspond with actual motor rated speed parameter.
(2) Modified the problem of PID compensation (P08.17).
(3) Modified the problem of torque limitation (P03.00=7~10).
(4) Modified the auto-tuning function to improve precision of motor parameters.
(5) Modified the bug of 3-wire control which the frequency command is disappeared as P02.00=3.
(6) Modified the bug of LED display are overflowed as the oH1 fault triggered.
(7) Modified the description of items of duty selection parameter (P00.16).
(8) Modified the bug of restarting after fault action (P07.10).
(9) Modified the bug of OL error after OC or OV errors.
(10) Added the read only parameters P03.47, P03.48 and P06.43.
(11) Modified the bug of fault reset parameter P9.30 in GS2 mode.
(12) Modified the default display of user page which is output frequency as P08.00=00 in GS2 mode.
(13) Modified the problem of the fire mode function and Dix not functionality.
(14) Modified the definition and calculation of power degree function in P05.24~P05.30.
Version: 1.00.2
Details:
FW Version: V1.00.2 (P00.06= 1.00)
Date Code: 20295 (P00.50= 20295)
Changes:
(-) Optimized warning temperature of NEMA4X models.
(-) Added the parameter Pr00-18 to display GS20 or GS20X.
(-) Modified the label of the group 14 to be "PROTECTION(2)"
(-) Modified the duplication function of parameter in GS2 mode. Eliminates SE2 error after parameter download.
(-) Hidden the parameter Pr09-64 reserved parameter.
Version: 1.00
Details:
GS20(X) Drive-Initial Production version release
FW version 1.00.1 (P00.06 = 1.00)
Date code = 20111 (P00.50 = 20111)