Latest shipping version:
Recent Firmware History:
Version: 3.6.004
Details:
Version 3.6.004 March 25, 2022
1. Field upgrade from any previous version to Version 3.6.004 requires a two-step upgrade procedure. Refer to the instruction document zipped with the firmware files.
2. After upgrading to Version 3.6.004, future firmware upgrades will use file extension “.ky”
NOTE: version 3.6.003 is not available to upgrade gateways in the field.
Version 3.6.002 (February 2022) bug fixes:
1. turns off the DHCP server that appears in versions 3.5.019 and 3.6.001
2. Makes the Hardware factory restore and User Interface factory restore behaviors consistent
3. Under some circumstances an abnormal restart occurs after a long run time
NOTE: versions 3.5.019 and 3.6.001 are not available to upgrade gateways in the field.
Version 3.6.001 (August 2021) improves communications at 300, 600 and 1200 Baud
Version 3.5.019 (July 2021) supports RTS flow control
Version: 3.6.001
Details:
It is not possible to field upgrade to version 3.6.001
Version: 3.5.019
Details:
It is not possible to upgrade any device in the field to firmware version 3.5.019 whether a gateway is downgraded from version 3.5.019 to an earlier version, or if a gateway shipped with an earlier version.
Bug Fix:
Change Flow Control to RTS Control in the Serial Settings configuration options
Version: 3.5.019
Details:
It is not possible to upgrade any device in the field to firmware version 3.5.019 whether a gateway is downgraded from version 3.5.019 to an earlier version, or if a gateway shipped with an earlier version.
Bug Fix:
Change Flow Control to RTS Control in the Serial Settings configuration options
Version: 3.5.013
Details:
1. In transparent mode, serial ports of gateway can’t get data after communication failed for one hour
2. Modify the prompt for input value in the added device configuration window in Agent mode
Download available from webstore firmware downloads page
Version: v3.5.012
Details:
1. Fix a TCP re-connect issue characterized by the serial port won’t reply “Gateway
Target Device Failed to Respond” when Gateway’s Ethernet port is down.
2. Disable port22 and 23 by default. If firmware is subsequently downgraded to version 3.5.007 (the only version prior to 3.5.012) the ports will remain disabled by default.
3. Disable NTP
4. General improvements to:
a. Help file text and help file icon
b. Device Information, Operating Settings and Serial Settings pages
5. Change Load Factory Default behavior so Reset isn’t a separate step
6. Auto refresh Message List screen
7. Add support for the following Modbus function codes under transparent mode:
0x07
0x08
0x16 (22)
0x17 (23)
0x0B (11)
0x0C (12)
0x11 (17)
0x14 (20)
0x15 (21)
0x18 (24)
0x2B (43)
8. Add Diagnostics page